Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
At first get an overview if there are changes in the update catalog at all and if yes, how many and of what kind.
Furthermore it is relevant, how far the LinkDB datasets can be automatically assigned (mapped) in a mapping process despite possible changes.
If the automatic mapping process could be successfully performed, the release can be performed after a simple check.
If the automatic mapping process war not successful, the affected projects must be assigned to LinkDB datasets by using search functionality.
The following information sources are available to determine the most effective approach.
Under PARTadmin -> category Catalog update -> Offline -> Check -> tabbed page Status you will get a list of all projects with information on changes.
Under PARTadmin -> category Catalog update -> Offline -> Compare you will see a Catalog comparison with directory structure and table. Changes of directory structure and name changes can be seen in the comparison at once.
On this see Section 5.15.2.1.4, “ PARTadmin - Check | Compare | Install”.
On this see Section 5.15.2.1.4, “ PARTadmin - Check | Compare | Install”.
After the update installation you can find further helpful information in the PARTlinkManager with the help of the values from columns ACTIVE_STATE and REQUESTED_STATE.
On this see Section 5.15.2.1.5, “ PARTlinkManager - Important notes on procedure”.