powered by CADENAS

Manual

Manual

3.3.12.4.1. General

PDMLINK_TargetFolder

With the option PDMLINK_TargetFolder the server onto which is to be checked-in is set. You must indicate the complete path including the folder. The path must be entered as follows:

wtpub://<Server Name>/<Products, Libraries, Projects,...>/<Context Name>/<Folder>

Example:

PDMLINK_TargetFolder=wtpub://192.168.1.216/Libraries/Lib1/SubFolderLib1

[Important] Important

If a folder is specified, it must also exist. The same goes for the library.

In addition you have the PLM_DoCheckin option. If this option is set to '0', then the check-in will not start automatically.

If this option is deactivated the PDM IDs should also not be shown. See ???.