powered by CADENAS

Manual

Manual

1.1.7.3.1.2.  Use FLM server

Optionally you have the possibility to connect the current computer with a FLM server and to get a license from there.

Hereto activate the checkbox Use FLM server. Once the checkmark is set a search for available FLM servers is automatically performed and these are displayed in the dialog box Select FLM server....

Select FLM server...

Select FLM server...

Select the desired FLM server and confirm with OK.

[Note] Note

The FLM server administration happens in the category FLM server. On this also see Section 1.1.7.4, “ FLM server ”.

Furthermore you have the following options in addition:

  • Restart scan for FLM servers

  • Manually specify FLM server...

    If a firewall blocks, you can manually specify the FLM server.