powered by CADENAS

Manual

Manual

5.20.5.6.4. Change NB via vbs scripting

If the options in the entry field do not suffice, you can generate a reference to a vbs script and work with complex conditions.

Set the entries under Standard name, Standard name (short) or BOM name.

In the example, the script is called nb.vbs and is located under …/setup/scripts/common.

The opened function is here called "ruletable".

function ruletable(table,calced_row,orgNB)
  result=""
  mmrow=cint(calced_row)
  if mmrow >= 0 then
     tmp=table.NN
     normbezeichnung=table.rows.item(mmrow).resolvevariables("$NB.",0)

'0.************************************************
    pos=Instr(1,normbezeichnung,"DIN")
    if pos = 1 then
       result=tmp+"_"+table.rows.item(mmrow).resolvevariables("$NENN.$MAT_NAME.",0)
    end if

'1.************************************************
    if tmp="DIN 912" then
       result="ISO4762abcd"+"_"+table.rows.item(mmrow).resolvevariables
       ("$NENN.$MAT_NAME.",0)
    end if

'2.************************************************
    if tmp="DIN 2448" then
       result="DIN 2448"+"_"+table.rows.item(mmrow).resolvevariables
       ("$D._$S._$L.___$MAT_NAME.",0)
    end if

'3.************************************************
    if tmp="DIN 2576" then
       result=tmp+"_"+table.rows.item(mmrow).resolvevariables
       ("$NENN._$D1.$MAT_NAME.",0)
    end if

'4.************************************************
    pos=Instr(1,normbezeichnung,"FAG")
    if pos >= 1 then
       result=table.rows.item(mmrow).resolvevariables("$NB.",0)
    end if

'5.************************************************
    pos=Instr(1,normbezeichnung,"EO EL L-Verschraubung mit Dichtkegel")
    if pos >= 1 then
       result=table.rows.item(mmrow).resolvevariables("$ERP_PDM_NUMBER.",0)+
       "-EL"+table.rows.item(mmrow).resolvevariables("$ROHR.$S.",0)
    end if

'6.************************************************
       if tmp="DIN 7993-B 2" then
       result=table.rows.item(mmrow).resolvevariables("$ERP_PDM_NUMBER.",0)+
       "-A"+table.rows.item(mmrow).resolvevariables("$D1.",0)+"---DIN7993"
    end if

' *************************************************

    if result="" then
      result=orgNB
    end if

  end if
  ruletable=result
end function
[Note] Note

For self-created vbs files, a special license is required.

You may only use the nb.vbs script if you enter the value of the key NBMODULE to nb in the configuration file plinkcommon.cfg in the Block Common in PARTadmin.