Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
By default, ERP is not supported for single parts inside assemblies. If a single part of an assembly is selected in the docking window Assembly and the button Add dataset to link database is clicked, then an error message is displayed pointing out the following configuration:
$CADENAS_SETUP/plinkcommon.cfg
[PARTdataManaager] UseErpForAssPart=0
If workflows shall be established where the ERP status of single part and assembly has to be taken into account , then set the key UseErpForAssPart to 1.
Under Extras menu -> Preferences... -> Assembly -> Show single parts tables in assembly tables you can find the setting in the user interface.
With the use of Scripting specific evaluations can be managed.
Assembly docking window with ERP functionality - example
The following example shows the possible operation mode with assemblies with ERP/PDM integration. The specific operation mode must be determined company internal.
The following displays refer to the assembly table project in the $CADENA/training directory under Assembly/hinge.