powered by CADENAS

Manual

Manual

2.3.2.7.1.3.  Key "COMMAND_SHOW_PSOLPartConnect"

ASSEMBLY DESIGN Toolbar - Activate the command that should be loaded at startup and set the value on "Yes". If a key is disabled the code and command will not be available in CATIA.

Connections

COMMAND_SHOW_PSOLPartConnect

Connections section in PARTdataManager is opened.

[Note] Note

In order for the commands to be displayed in the PARTsolutions toolbar, you have to edit the respective keys starting with "MN_" in addition.