Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
With this program you can convert 3D files and create preview images in batch mode.
You can use "Scheduled tasks" in Windows. (Hereto no GUI is needed; ActiveX is possible!)
(When you call up
batchconvert.exe
without
parameter or with '--help' or with '-?', then the help with all possible
parameters is displayed.
The file batchconvert.exe
is found under:
C:\Program Files (x86)\cadenas\partsolutions\software\bin\x86\32\batchconvert.exe"
Call up happens in the following form:
batchconvert sourceDirName [--targetdir targetDirName] [--logfile logFileName] [--errorfile errorFileName] [--inputformats format1 format2 format3 ...] [--outputformats format3d formatImage] [--recursive] [--meshreduction] [--debug] [--imagewidth] [--imageheight]
C://abc/def/file1.prt C://abc/ghj/file2.prt C://xyz/stu/file3.prt
In order for the structure of source files to be mapped correctly at the target, the target path is detected as follows:
At first the directory with the deepest path with the characteristic that it contains all files from the list is determined .
Then this common path is replaced by the specified target path.
Focusing on the first two lines the deepest common path would be "../abc" and focusing on all three lines it would be "C://".
Supposed target path would be:
C://target
C://target/abc/def/file1.stl C://target/abc/ghj/file2.stl C://target/xyz/stu/file3.stl
The common path may not be empty, especially all files have to be in the same drive or computer in the network.
Ergo the following is not possible:
C:/abc/file1.stl D:/abc/file2.stl
Or
\\10.10.0.75/dir1/file1.stl \\10.10.0.159/dir1/file2.stl
Description of the single parameters:
--(l)ogfile: Log file, which contains a list of all converted files
The file contains the complete paths to all converted output files as \t separated CSV.
One line for each input file: col1=inputFilePath, col2=outputPathFormat1, col3=…)
--(e)rrorfile: Error file, which contains a list of all files where an error occurred.
The file contains the complete paths to the faulty input files.
--(i)nputformats: Input formats to scan for in the source directory
The following list exemplifies a selection of formats. Using the '--listformats' or '-l' you can output all formats in order to detect the correct names for the call up.
--(o)utputformats: Output formats
--(m)eshreduction: The geometric part complexity is reduced. Stating this parameter cannot damage anything and makes sure that the geometric index can be correctly created. But in any case a respective message is outputted in the log file.
--(d)ebug: An enhanced version is displayed in the command window.
In order for
the program to be prevented from converting ALL files again, the
parameter --ignorenotmodified
can be
used.
--ignorenotmodified
Files which have not been modified are ignored at a new conversion.
Files which have been modified are converted again and preview images are generated.
If only --overwrite
is active,
existing files are always overwritten.
If neither
--overwrite
nor
--ignorenotmodified
is active, existing files are not overwritten.
--deleteinput
Deletes the original files.
--defaultpreview3d
Default file, if the conversion fails. The file must already have the target format.
--defaultpreview
Default preview image, if the preview image cannot be created. If already the conversion of the 3D file fails, this preview image is used - if set. Otherwise the preview image is created from the default 3D file. Also here the image must have the same format as the created preview images.
batchconvert "C:\src" --targetdir "C:\target" --meshreduction --recursive --outputformats BMP PARTJAVA --inputformats STLFILE --logfile C:\logfile.txt --errorfile c:\errorfile.txt
batchconvert "C:\src": -t "C:\target" -m -r -o BMP STL -i NATSOLIDEDGEPARTST2 NATSOLIDEDGEASMST2 -l C:\logfile.txt -e c:\errorfile.txt
A detailed description of geometry import via GUI is found under Section 1.1.3.4.4.4, “ Import geometry data ”.