powered by CADENAS

Manual

Manual

1.1.6.6.6.1. Block [SettingsIndexTree] - Settings for part selection

Settings for part selection in PARTdataManager:

1.1.6.6.6.1.1.  Key "GenerateMissingTopologyData" - Suppress regeneration of missing topology data

In the standard catalog, for example, fingerprints only exist for a few lines. Now, when setting the option Topology values, the generation of missing topology data is processed by default.

If this is not wanted, set the following:

$CADENAS_USER/psolopt.cfg

[SettingsIndexTree]
GenerateMissingTopologyData=0

Set the above key with value 0.

Now the respective values remain empty

1.1.6.6.6.1.2.  Key "ClickableVariables" - Search result - Clickable variables and values

You can configure, whether the variables and their values shall be clickable in search results.

When clicking on a variable a variable search is directly performed, value based on it.

When clicking on a variable the dialog box Variables search opens.

In the exemplary figure variable searches with D=6 and L=30 have been performed.

In the exemplary figure variable searches with D=6 and L=30 have been performed.

$CADENAS_USER/psolopt.cfg

[SettingsIndexTree]
ClickableVariables=1 (Default)

Value range: 0 (not clickable) / 1 (clickable)

1.1.6.6.6.1.3.  Key "SearchFilterHint_MaxResults" - Search result filtered - Control of message

If filters such as Preferred rows on/off are enabled, this affects (reduces) the search results. Compare Section 3.1.2.7.2.3, “ Use preferred rows filter ” in PARTsolutions / PARTcommunity4Enterprise - User manual.

Via key SearchFilterHint_MaxResults you can adjust, whether a respective message is displayed at all or which number of hits is displayed below.

"Note: preferred rows are enabled! You only get hits from projects with at least one ERP assignment. The number of hits increases likely, if you disable it in the toolbar."

$CADENAS_USER/psolopt.cfg

[SettingsIndexTree]
SearchFilterHint_MaxResults=

Value range:

  • -1: No message is displayed

  • 0: A message is only then displayed, when there are no hits at all (default).

  • 1-5: When there are <= 1 to 5 hits, then a message is displayed.

1.1.6.6.6.1.4.  Key "ShowDisplayRanking" - Search results: Placement number

At all search methods the placement number is displayed in the first column.

The placement number can be displayed or hidden via configuration file.

Configuration file: psolopt.cfg

[SettingsIndexTree]
ShowDisplayRanking=0/1

1: Placement number on (default)

0: Placement number off

1.1.6.6.6.1.5.  Key "EnableOverlayPopup" - Search results: Popup window

In the following cases additional information is found in the popup window:

  • Table cell too small

  • Hit happened because of matches in another language

  • Hit happened because of matches in the path

Topology search with "Any parameter" delivers a lot of values. In order for all values to be displayed, click into the cell.

Topology search with "Any parameter" delivers a lot of values. In order for all values to be displayed, click into the cell.

If the following key is not available, then you may add it yourself.

[SettingsIndexTree}
EnableOverlayPopup=0

Default value = 1 = On = Popup window activated

1.1.6.6.6.1.6.  Key "LINKCLASSLIST" - Adjust dialog area "Links"

Block [SettingsIndexTree]

Key: LINKCLASSLIST

Relation: PARTdataManager -> Dialog area Links -> displayed options in the list field

Adjust the comma separated values as desired.

1.1.6.6.6.1.7.  Key "SHOWUSECASESDOCK" - Use Cases (Online)

PARTdataManager -> Context menu of any toolbar or menu bar

Indicates whether the dock Use Cases (Online) should be shown.

$CADENAS_USER/psolopt.cfg

[SettingsIndexTree]
SHOWUSECASESDOCK=1

Value range: 0/1

If Use Cases (Online) is principally activated, nevertheless the user can decide, whether the feature shall be active or not.

1.1.6.6.6.1.8.  Key "ShowInstallHistory" - Show/hide Installation history

You can show or hide the installation history.

[SettingsIndexTree]
ShowInstallHistory

Value range: yes/no

Tooltip: Changes / New files in the directory

Tooltip: Changes / New files in the directory

1.1.6.6.6.1.9.  Key "KeySynonyms" - Synonym editor

Using PARTsynonym you can define and manage synonyms.

Among other things, the synonyms you defined can be taken into account in PARTdataManager during the Full-text search.

This way you can find products, you otherwise wouldn't have found by reason of different notation (e.g. hexagon screw, hexagon head screw, hexagon head set screw, hexagon bolt, ...).

In PARTadmin, in order to enter data click on Start PARTsynonym!.

In PARTdataManager, check/uncheck the option in order to use the search database.

[SettingsIndexTree]
KeySynonyms=

Value range:

-1=disabled: The Search for synonyms pushbutton is not shown in the PARTdataManager.

0=turned off;

1=turned on

More information about the synonym editor can be found under Section 1.1.8, “ PARTsynonym ”.