Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
For the new generation of a part which is not yet covered in SAP there are two different processes:
Both processes are independent from each other, but are normally used together.
Depending on configuration each of the two processes can run "light" or "dark". But normally the SAP MM process runs "light" and the SAP PLM process runs "dark".
In the following the whole procedure is explained in general. Examples are found under Section 3.3.8.5, “New generation of DIS and Material - Examples”.
Release button for the creation of DIS and Material can be different in PARTdataManager. One possibility is the Export to CAD button for example.
PARTsolutions starts the SAP PLM interface in the background (dark) and fills fields such as:
PLM information is transferred back into the CADENAS LinkDB.
Together with the saving of the MM data record the MAT No. and other desired information fields are transferred back into the CADENAS LinkDB and displayed for all users