Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The configuration is performed under %CADENAS_SETUP%\ifagile.cfg.
In this section you should not perform any changes normally. It just references to the next two sections.
[AttributeMapping(is3d)] Attr_Content_00 =MAPPINGTOAGILE Attr_Section_00 = MAPPINGTOAGILE Attr_Content_01 =LINKDB_RETURN_MAPPING Attr_Section_01 =LINKDB_RETURN_MAPPING
Basics on attribute mapping are explained under Section 2.2.4, “Attribute mapping ”.
Return-Mapping: AGILE -> PARTsolutions PLINKDB
In the section [LINKDB_RETURN_MAPPING(isRootDoc)] you can adjust, how and where the Agile attributes shall be transferred to the link database.
<TABLE>.<COLUMN>=?<VALUE>
<TABLE> stands for "ERPTABLE" or "LINKTABLE".
<COLUMN> stands for all columns excluding ERP_PDM_NUMBER.
<VALUE> is the value on which the column <TABLE>.<COLUMN> is set.
It can contain a placeholder like %MATNR%, which is set to the correct value by the PDM interface.
bla_%MATNR%_blub -> bla_12345_blub
All valid, accessible AGILE database entries
T_DOC_DAT.DOCUMENT_ID
For columns of the type "VARCHAR" the whole value expression <value> has to be embedded in single quotation marks (see following examples).[48]
[LINKDB_RETURN_MAPPING(isRootDoc)]
ERPTABLE.MATNR=?"'%MATNR%'"
ERPTABLE.SAPSTATUS=?"'%T_DOC_DAT.DOCUMENT_ID%'"
ERPTABLE.TESTVC=?"'%T_DOC_DAT.C_ID%'"
ERPTABLE.TESTINT=?"555"
Mapping: PARTsolutions PLINKDB -> AGILE
In the section [MAPPINGTOAGILE] you can adjust, where PARTsolutions attributes (link database) (right side) have to be transferred to Agile (left side).
[MAPPINGTOAGILE]
T_DOC_DAT.DOC_NAME=NAME
T_DOC_DAT.DOC_NAME_GER=NAME_DE
T_DOC_DAT.DOC_NAME_ENG(isRootDoc)=?"NAME_EN"