powered by CADENAS

Manual

Manual

2.3.1.7.1.1. As of version 2011

During installation the following files are registered:

(RegisterAcadxxPlugin.exe)

  • AutoCAD 2011:

    [CADENAS]\iface\autocad\2011_32\ifacad2011_32.dll

    [CADENAS]\iface\autocad\2011_64\ifacad2011_64.dll

  • AutoCAD 2012:

    [CADENAS]\iface\autocad\2012_32\ifacad2012_32.dll

    [CADENAS]\iface\autocad\2012_64\ifacad2012_64.dll

  • etc.

These DLLs are automatically unregistered during deinstallation.

A manual registration can be done via the register.bat file.

RegisterNoAutoload.bat:

RegisterNoAutoload sets security entries for the plugin at the operating system. However the plugin is not automatically loaded while launching AutoCAD.

In order to manually load the AutoCAD command "netload" can be used.