powered by CADENAS

Manual

Manual

1.1.6.7.14.  material_assign.cfg (with ERP integration)

In the configuration file material_assign.cfg you can define, which materials shall be displayed in PARTdataManager, in the dialog box new ident-no..

When exporting to the CAD system the PARTsolutions material is mapped onto the CAD system material, so that the physical properties can be calculated in the CAD.

More information

Information on the transfer of the material attribute to the CAD system is found under Section 2.2.5, “Material mapping ”.

Information on the integration of the material into the file name is found under Section 2.2.2.2, “File name: set generation options ("FileName" key) ”. Per default an available material information is overtaken into the file name.