powered by CADENAS

Manual

Manual

4.16.3.5.2. Changed standard name

If in a project the standard name (NB) has been changed, then in the section Catalog all project lines, the project itself and the superordinated directory are marked with the orange exclamation mark . The exclamation mark overlays the respective base symbol (directory , project , line ).

Once in the directory structure a line is selected, in the section Line mapping the single variables and the table are displayed.

In the variable line NB you can see the change.

Now you have two possibilities:

Approve assignment

(Mapping correctly despite of NB changes)

Revoke assignment and save changes (Mapping not correctly)

Then in the index tree the respective symbols or are displayed.