powered by CADENAS

Manual

Manual

2.2.2. Set file name ("FileName" key) and pool path ("poolpath" key)

Due to the meaning of file name and pool path settings these two keys have their own dedicated section.

[Note] Note

With the two keys PoolPath and FileName you can set the structure of pool (flat or with subdirectories) and the creation of file name.

[Note] Note

Use the appropriate configuration file for your CAD system.

It is found under PARTadmin -> Category -> PARTsolutions -> Configuration files -> $CADENAS_SETUP -> if<cad name>.cfg.

PARTadmin -> Category -> PARTsolutions -> Configuration files -> $CADENAS_SETUP -> if<cad name>.cfg

PARTadmin -> Category -> PARTsolutions -> Configuration files -> $CADENAS_SETUP -> if<cad name>.cfg

[Note] Note

For a better understanding of the examples please absolutely read Section 2.2.1.3, “Variable values - functions ”. Basic concepts are explained under Section 2.2, “CAD encompassing information ”.

Thereof you can deduce how to adjust the examples according to your needs.

[Important] Important

Are you a new customer? Then you may simply use the default settings or make adjustments if desired.

When you like to reuse CAD files in PARTsolutions V11 which have been created with PARTsolutions V8.1 catalogs then you have to make sure that these parts can be found in the V8.1 pool.

Basically this means that the directory hierarchy (flat pool or sub-directories) and the file name must be kept.

Especially regard Section 2.2.2.3, “Reuse the V8.1 pools after migration to V9 ”.