powered by CADENAS

Manual

Manual

2.3.3.2.8.  Key "APPLY_PART_MATERIAL_TO"

Applies the material on either the part, the body, both, or none.

Example:

APPLY_PART_MATERIAL_TO=Part

Value range:

  • ""

  • part

  • body

  • none

On this also compare the following keys:

  • CATMaterial File

    The key represents the name of CATMaterial File which is taken into account for created Parts. If the Metafile contains some Material information, the name of Material is searched in the specified CATMaterial File and if found it will be applied.

    Examples:

    [CreationOptions]

    MaterialFile(is3dpart)=MaterialFile.CATMaterial

    [CreationOptions]

    MaterialFile(is3dpart)=?Aplication.ResolveEnv("K:\\DS\\B18\\win_b64\\startup\\materials\\Catalog.CATMaterial")

  • StdMaterial(is3dPart)

  • Material(is3dpart)

    Name of the material from the MaterialFile, read from the part physical properties.

    Example:

    Material(is3dpart)=?GetObject("iface.calcnameservice").start(0).Format("<CLASSPROP ( cns,CNSPHYPROP,CNSMAT ) > ").value()