powered by CADENAS

Manual

Manual

2.3.3.7. Commands to adjust behavior/visibility of PARTsolutions interface menu and workbenches

In the following you can find details on how to adjust the behavior/visibility of PARTsolutions interface menu and workbenches.

Visibility and activation of menus, workbenches, buttons

Basic settings are made under $CADENAS_SETUP/ifacecommon.cfg -> Block [UI] -> especially keys starting with "MN_". Settings can be overwritten in $CADENAS_SETUP/ifcatia.cfg -> Block [UI] by a same-named key. A detailed description on how the commands in ifacecommon.cfg and ifcatia.cfg interact is found under Section 2.2.1.6, “Configuring PARTsolutions interface menu and toolbar ”.

[UI]
MN_DisplayText_50=Einfügen 3D
MN_HelpText_50=3D-Teil oder -Baugruppe aus einer Bibliothek einfügen
MN_SmallIcon_50=:/cadresource/icons/paste3d_16x16.png
MN_LargeIcon_50=:/cadresource/icons/paste3d_24x24.png

etc.

[Note] Note

As of V11 SP3 visibility and activation is effected by the same keys. This happens in the course of adapting functionality of all CAD interfaces.

ifcatia_start.cfg is not used anymore. So with V11 SP3 there is no representation for this functionality, meaning affecting the time of loading functions is not possible currently.