powered by CADENAS

Manual

Manual

2.3.5.1.1.  Key "poolpath" - Set storage path for PARTsolutions parts

In the key poolpath, set the directory where all parts created by PARTsolutions shall be stored.

On this also see:

You can use both the standard pool path and a library path from the Inventor project as pool path.

Default:

poolpath(isCreaOptNotSet)=?_FORMAT_0("$CADENAS_DATA/pool/inventor/<PREFIXLIST(/)>").value()

In order to change the standard pool path, do the following:

  1. In the Inventor, open the Projects dialog page.

    Apply a library with the desired export path for the PARTsolutions parts.

    Apply library

    Apply library

    [Note] Note

    As long as the library keeps the same name (in this case "POOL"), different paths can be set on it in different projects.

  2. Open PARTadmin -> Category -> $CADENAS_SETUP -> ifadeskinv.cfg -> Block CreationOptions(is3d) -> key pool path(isCreaOptNotSet)

    Change the field entry:

    ?GetObject("iface.contextservice").GetVariable("UserApp").GetActiveProjectPath("POOL")

    (In the last brackets there is the library name.)

    Or alternatively:

    ?GetObject("iface.contextservice").GetVariable("UserApp").GetActiveProjectPath("POOL")
    +GetObject("iface.calcnameservice").start(0).Format("/<PREFIXLIST(/)>").value()

    <PREFIXLIST(/)>: At projects with several prefixes these are automatically prefixed in the path, separated by a slash (e.g. Norm9 [Standards], Kernloch [Core diameter]).

    Change key for pool path in PARTadmin

    Change key for pool path in PARTadmin

  3. Now the library can be used as pool path.

    Library "POOL" is shown for selection

    Library "POOL" is shown for selection