powered by CADENAS

Manual

Manual

1.7.5.19.4.20.  Keys "TABBAR_ORDERABLE" and "TABBAR_ORDER" - Tabs: Allow drag & drop and tab order

With the help of these two keys you can determine the sequence of the content tabs in PARTdataManager.

[Note] Note

Keep in mind: It's just to determine the sequence not the visibility. Other keys may interact in addition.

  • TABBAR_ORDERABLE:

    • TRUE

      The user can change the sequence via drag & drop.

      When finishing PARTdataManager the sequence set by the user is saved in the user directory.

      For the very first start (no user directory existing yet) the sequence specified under TABBAR_ORDER is taken.

    • FALSE

      Drag & drop is not possible. This is precondition to make the key TABBAR_ORDER work permanently.

  • TABBAR_ORDER:

    The following values are available:

    • Assistant: ASSISTANTVIEW

    • Part selection: PARTSELECTIONDEFAULT

    • Document scan: DOCSCANDEFAULT

    • Part view: PARTVIEWDEFAULT

    • Part comparison: PARTCOMPAREDEFAULT

    • Classifications: CLASSIFICATIONSDEFAULT

    • Favorites: FAVORITESDEFAULT

    • History: HISTORYDEFAULT

    • Cloud Navigator: CLOUDNAVIGATORDEFAULT

    • Search results: SEARCHRESULTDEFAULT