Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
As of version 9.08 there are some changes concerning storage location and files:
The Geo Index and the Topology Index are saved separately now.
The new Geo
Index is found in the subfolder geoindexv2
(beneath the "old"
geoindex
), the Topo
Index in the folder topoindex
.
The following files are found in the directory geoindexv2:
This file contains the fingerprints for the single algorithms.
This file contains information on the part, which is only relevant at the generation of the fingerprints, meaning that this information has not to be read during the search.
This file contains the Linear Index for the single search templates.
geomsearch.ofm: This file contains a mapping of project paths on the internal IDs of the Geo Index.
In a certain mode the updates of the Geo Index are not directly integrated in the Geo Index, but saved in special files, in order to accelerate the procedure. More information on this is found under Section 1.7.5.9.10.2.3, “ Creation of Geo and Topo indices”. Therefor the following files are used:
geomsearch.ucidb: Contains information of changes, which are not relevant for the search itself.
geomsearch.uop: Contains all needed information in order to be able to integrate the fingerprint changes into the Geo Index. Possibly the Geo Index is just being worked on.
In this case another file is found in this directory:
geomsearch.lock: Prevents from accessing the Geo Index during writing on it.
General settings under $CADENAS_SETUP/geomsearch.cfg are found in the section [settings].
Determine, which Geo Index shall be used for searching. Possible values are:
Determine, which Topo Index shall be used for searching. Possible values are:
Control, whether the old or the new index shall be created. Possible values:
Shall the Linear Index be created again at the conversion? Possible values:
For the creation of indices there are three basic possibilities:
Update of the existing index (working on copy). Here the available index can also be an old Geo Index. This, then is automatically converted.
Update of the existing index (working with special update files). Makes sense, if there are only little changes at large catalogs.
Variant 3 is much quicker the variant 2, especially at large catalogs.
Variant 3 has the disadvantage, that the search becomes slower with each new update. That's why it makes sense to update the index using mode 2 from time to time, because then the updates are completely integrated in the index.
The Pivot elements of the Linear Index are not calculated anew in variant 3. Possibly this can have a negative effect on search times.
Basically applies that the 64 Bit variant has a better performance (similar as with the migration).
During the generation of the indices the directories of Geo and Topo index are locked. The variants 1 and 2 are working on a temporary copy. Here the directory is only locked for writing access at the beginning. This means, that the index can still be read. The index has to be locked for reading access only for a short moment, when the old files are deleted and the temporary files are renamed. The 3rd variant does not work on a copy. That's why the access is locked during the whole update.
Via key
ThreadCountForLinearIndexCreator
in the section settings_32
or settings_64
is can be
determined, how many threads have to be used for the creation of the
Linear Index. For value "-1" the existing number of cores is used.
Possibly each thread needs some hundred MB working memory. That's why,
too high values make no sense for 32 Bit.
[settings_32] ThreadCountForLinearIndexCreator=2 [settings_64] ThreadCountForLinearIndexCreator=-1
For Geo and
Topo index the are 3 different modes for performing the search for
each, depending on the entry under geomsearch.cfg
, section
settings
(see above).
Furthermore the Linear Index is also used for the sketch search as of version 9.08 in order to reduce search times.
All caching settings can be set differently for the PARTdataManager 32 Bit and 64 Bit variant.
LinIndexCacheSize: Cache size for the Linear Index in KB
Choose the value in a way, that it is not maximally used.
If this is
not possible, then set a small value for the superordinated storage
(SampleLineCacheSize
).
[CACHEV2_GEO_SEARCH_32] LinIndexCacheSize=100000
[CACHEV2_GEO_SEARCH_64] LinIndexCacheSize=300000
OffsetCacheSize: Cache size for the Offset index in KB
Choose the value in a way, that it is not maximally used.
If this is
not possible, then set a smaller value for the superordinated storage
(SampleLineCacheSize
).
[CACHEV2_GEO_SEARCH_32] OffsetCacheSize=50000
[CACHEV2_GEO_SEARCH_64] OffsetCacheSize=150000
GeoIndexV2CacheSize: Number of Geo indices, which can be opened at the same time.
Set the value in a way, that it is according to the maximal number of catalogs.
[CACHEV2_GEO_SEARCH_32] GeoIndexV2CacheSize=1000
[CACHEV2_GEO_SEARCH_64] GeoIndexV2CacheSize=1000
SampleLineCacheSize: Cache for fingerprints in KB
Cache for all Threads (is normally according to the number of all processor cores altogether)
[CACHEV2_GEO_SEARCH_32] SampleLineCacheSize=100000
[CACHEV2_GEO_SEARCH_64] SampleLineCacheSize=500000
LogFileName: Here the log information is saved, if not empty. See below.
Set the key yourself, if not existing.
[CACHEV2_GEO_SEARCH_32] LogFileName=c:\log\cachev2_geo_search_32.log
[CACHEV2_GEO_SEARCH_64] LogFileName=c:\log\cachev2_geo_search_64.log
The setting can be used for Server environments in order to exclude catalogs or to load only special catalogs.
#:VALS_S #:HELP;default;Include catalog, if the expression matches. PreloaderIncludeRegexPos= #:HELP;default;Include catalog, if the expression doesn't match. PreloaderIncludeRegexNeg= #:VALS_S #:HELP;default;Exlucde catalog, if the expression matches. PreloaderExcludeRegexPos=.*copyright\.prj$|.*_qa$|.*_dev$ #:VALS_S #:HELP;default;Exclude catalog, if the expression doesn't match. PreloaderExcludeRegexNeg=
Also compare $CADENAS_USER/varsearch.cfg -> [VariableSearch:Path]:
The setting
under geomsearch.cfg
is used to cache the geometrical index, the one under $CADENAS_USER/varsearch.cfg
[VariableSearch:Path]
is used to cache the index for variable
and full-text search.
ObjectDataCacheSize: Cache for Topo data nodes
Especially important for the migration.
[CACHE_TOPO_SEARCH_32] ObjectDataCacheSize=200000
[CACHE_TOPO_SEARCH_64] ObjectDataCacheSize=1000000
IndexCacheSize: Cache for indices on the Topo data.
Especially important for the Topo search.
[CACHE_TOPO_SEARCH_32] IndexCacheSize=200000
[CACHE_TOPO_SEARCH_64] IndexCacheSize=500000
LogFileName: Here log information is saved, if not empty. Also see Section 1.7.5.9.10.2.6, “ Log file evaluation - Find best settings”.
Set the key yourself, if not available.
[CACHE_TOPO_SEARCH_32] LogFileName=c:\log\cachev2_topo_search_32.log
[CACHE_TOPO_SEARCH_64] LogFileName=c:\log\cachev2_topo_search_64.log
With the help
of the log files (key LogFileName
), mentioned above,
the search settings (thus the search behavior) can be optimized for the
existing data. You can learn from the log file how full the respective
cache is and how often an element has really been in the cache at each
access (Cache hits).
Search from Do 12. Dez 22:41:09 2013 Thread: 0xce8 Geometrical index cache: Capacity of the cache: 1000 In use: 18 (1.80%) Free: 982 (98.20%) Accesses to the cache: 6489 Cache hits: 6471 (99.72%) Cache misses: 18 (0.28%) Linear index cache: Capacity of the cache: 100000 In use: 4962 (4.96%) Free: 95038 (95.04%) Accesses to the cache: 1932 Cache hits: 1615 (83.59%) Cache misses: 317 (16.41%) Offset index cache: Capacity of the cache: 50000 In use: 1617 (3.23%) Free: 48383 (96.77%) Accesses to the cache: 7033 Cache hits: 6716 (95.49%) Cache misses: 317 (4.51%) Sample lines cache: Capacity of the cache: 100000 In use: 82785 (82.78%) Free: 17215 (17.22%) Accesses to the cache: 16840 Cache hits: 10985 (65.23%) Cache misses: 5855 (34.77%)
Some notes for the interpretation of data:
Possibly the log file is not updated until a further search is performed.
In order to make effective settings with the help of the log file, it is important to perform several searches, which are adequate to the normal user behavior, for example concerning the selection of search templates, sketch search or 3D search, but also concerning the selection of search parts.
The information on cache hits and cache misses, which are readout with each search, are cumulative.
The data are loaded into the cache not until the first access has been performed. That's why the first access on data is always a cache miss. The more searches have been performed, the less cache misses should occur.
You can access the Topo values in the following way:
' main class to manage topology set topoManager = CreateObject("cnstools.topomanager") ' fetch root node of topology tree set catalogRoot = topoManager.findCatalogRoot("cat/norm/din") stdprint("Number of project in din: " & catalogRoot.childCount) ' fetch project node set prjNode = topoManager.findProjectNode("cat/norm/din", "anlagenbau/armaturen/ din_11864_1_a_asmtab.prj") stdprint("Number of lines in anlagenbau/armaturen/din_11864_1_a_asmtab.prj: " & prjNode.childCount) ' fetch line node set lineNode = topoManager.findLineNode("cat/norm/din", "anlagenbau/armaturen/ din_11864_1_a_asmtab.prj", 20) ' helper to recursively print all the attributes of a node sub printAttributes(node, indent) stdprint(indent & node.name) c = node.childCount for j = 0 to c - 1 printAttributes(node.child(j), indent & " ") next a = node.attributeCount for j = 0 to a - 1 set attr = node.attribute(j) value = attr.value valueAsString = "" set attrType = attr.type if attrType = "doubleVec" then n = value.count for k = 0 to n - 1 if k > 0 then valueAsString = valueAsString & ", " end if valueAsString = valueAsString & value.item(k) next else valueAsString = value end if stdprint(indent & " " & attr.name & ": " & valueAsString) next end sub ' print all attributes for a line stdprint("Recursive list of all attributes in line 20:") stdprint() printAttributes(lineNode, "") stdprint() ' print all attributes for a stl file stdprint("Recursive list of all attributes in stl:") stdprint() set stlNode = topoManager.createNodeFrom3DFile("D:/stl/1 stl/001952002.stl", "STLFILE") printAttributes(stlNode, "") ' print all attributes for a prt file stdprint() stdprint("Recursive list of all attributes in prt file:") stdprint() set prtNode = topoManager.createNodeFrom3DFile("D:/stl/ein paar proe-Dateien/ 1202t4100_gen.prt.1", "NATWILDFIREPART 5 32 BIT") printAttributes(prtNode, "") ' print all attributes for a line (create fingerprints on the fly) stdprint() stdprint("Recursive list of all attributes in line 420:") stdprint() set lineNode2 = topoManager.createNodeFromProject("cat/norm/din", "anlagenbau/armaturen/ din_11864_1_a_asmtab.prj", 420) printAttributes(lineNode2, "") ' print all attributes for a project (create fingerprints on the fly) stdprint() stdprint("Recursive list of all attributes in project anlagenbau/armaturen/ din_11864_1_a_asmtab.prj:") stdprint() set prjNode2 = topoManager.createNodeFromProject("cat/norm/din", "anlagenbau/armaturen/ din_11864_1_a_asmtab.prj", -1) printAttributes(prjNode2, "")