powered by CADENAS

Manual

Manual

2.3.9.3.  Attribute mapping in SolidWorks

In the block AttributMapping(is3d), you can determine whether the PARTsolutions standard attributes (geometrical, NT, NN, LINA, etc.) and all fields in the link database (if an ERP connection exists) can be transferred to the CAD system, and if so, in which language(s).

In the following you can find the most important information for your CAD system. Basic information on attribute mapping can be found under Section 2.2.4, “Attribute mapping ”.

Once the attributes are transferred they are available on the dialog File information and in the List of Material.

"File information" -> tabbed page "Custom"

"File information" -> tabbed page "Custom"

PARTsolutions attributes in the BOM list table

PARTsolutions attributes in the BOM list table

Attribute mapping is controlled by the following blocks:

The following describes the individual blocks:

[Note] Note

For editing settings, admin rights are required!