powered by CADENAS

Manual

Manual

1.3.4.1.8.  PARTupdate - Notification on available catalog updates

PARTupdate automatically informs you on catalog updates via icon PARTupdate displayed in the task bar.

  • Without exclamation mark: Currently there are no updates available.

  • With exclamation mark: Updates are available.

When double-clicking on the icon the PARTupdate short info opens.

PARTupdate short info

PARTupdate short info

The number of downloadable catalogs and which in detail is displayed here.

  • Click here for details.

    When clicking on the button the dialog box PARTsolutions - Available catalogs opens with a list of all downloadable catalogs and catalogs which can be updated .

    Here you can get an overview which catalogs you would like to download or update.

    Here you can get an overview which catalogs you would like to download or update.

    When clicking on the button To the download selection PARTadmin opens in the category Catalog update -> Online.

    Detailed information on the Catalog update can be found under Section 1.3.4, “ Catalog update ”.

  • Click here, to select catalogs you want to download.

    When clicking on the button PARTadmin opens in the category Catalog update -> Online.

    Detailed information on the Catalog update can be found under Section 1.3.4, “ Catalog update ”.

Precondition for the icon display and respective functionality

If the option PARTupdate automatically start with Windows? had been activated in the installation, the icon is automatically displayed.[a]

PARTupdate automatically start with Windows?

PARTupdate automatically start with Windows?

[a] At the end of the installation the PARTupdate settings wizard is automatically launched.

Otherwise you can launch PARTupdate via Start menu (Start -> All Programs -> CADENAS -> PARTsolutions -> PARTupdate) anytime.

PARTupdate settings wizard

At the very first start the PARTupdate settings wizard is automatically launched so that you can determine certain modalities here.

Welcome to the PARTupdate settings wizard

PARTupdate settings wizard

PARTupdate settings wizard

Please specify the intervals which should be used to check for updates.

Automatic catalog update notification

Automatic catalog update notification

Please specify about which downloads you want to be informed.

Catalog update notification

Catalog update notification

Does your connection goes through a proxy? If you have not set it yet, then you can do it now.

Network settings

Network settings

On the last dialog page the result of the connection test is displayed.

Results

Results

Context menu commands

Context menu commands on the icon or .

  • Check For Updates:

    -> The short info is displayed. The same can be reached by a double-click on the icon.

    PARTupdate short info

    PARTupdate short info

  • Start Update Assistant:

    -> PARTadmin opens.

  • Settings:

    -> The PARTupdate settings wizard opens. Here you can change settings at a later time if needed.

  • Close:

    -> PARTupdate is finished and the icon in the task bar is not displayed anymore. You can start PARTupdate at a later time via Start menu.