powered by CADENAS

Manual

Manual

2.2.8.8.  Block [RAWMATERIALS]

Semi finished parts can be classified as such.

for desired projects, in PARTproject, under Edit project -> General -> Classification -> Attributes (CNS), the feature CNS_RAWMATERIAL is set on 1. See Section 5.13.5, “ Add projects to classification ” in eCATALOGsolutions Manual.

[Note] Note

In exceptional cases, Consulting can step in via configuration file and so declare certain directories/projects in this way.

Local changes in the project file are not target-aimed, because these will get lost at next catalog update. Changes should be performed centrally during modelling process.

[Note] Note