powered by CADENAS

Manual

Manual

2.3.6.2.  Attribute mapping in Creo / ProEngineer

PARTsolutions variables (geometric, NT, NN, LINA, etc.) and all fields in the link database (if an ERP connection exists) can be transferred to ProEngineer via attribute mapping.

These are then described on the Parameter dialog page.

ProE: Parameter

ProE: Parameter

For attribute mapping open the category CAD integration -> ProeWildFire in PARTadmin.

The attribute mapping is controlled via the following blocks:

The following describes the individual blocks:

[Note] Note

In order to be able to edit settings, admin rights are required!