powered by CADENAS

Manual

Manual

4.2.6.4.  Configuration file jdbc.cfg

The jdbc.cfg is for the database connection data, i.e. Server, Database, in particular the driver class and the URL for the jdbc driver to establish a connection to the database.

This file is organized in DSNs like the following:

# [PLINKDB]
#   #IP-adress or server name
# Server=
#   #Database name
# ServerDB=
#   #the jdbc driver class
# DriverClass=com.sap.dbtech.jdbc.DriverSapDB
#   #the complete URL for the jdbc driver
# URL=jdbc:sapdb://catia2.cadenas/PLINKDB

#Examples for different databases:
--------------------------------

#MSSQL with JTDS
#[PLINKDB_MSSQLJDBC]
#Server=136.230.230.214
#ServerDB=DB-test
#DriverClass=net.sourceforge.jtds.jdbc.Driver
#URL=jdbc:jtds:sqlserver://136.230.230.214:1433/PLINKDB

#Oracle:
#[PLINKDB_ORACLEJDBC]
#DriverClass=oracle.jdbc.driver.OracleDriver
#URL=jdbc:oracle:thin:@servername:1521:PLINKDB

#SAP-DB:
#[PLINKDB_SAPDBJDBC]
#DriverClass=com.sap.dbtech.jdbc.DriverSapDB
#URL=jdbc:sapdb://servername/PLINKDB

#MySQL:
#[PLINKDB_MYSQLJDBC]
#DriverClass=com.mysql.jdbc.Driver
#URL=jdbc:mysql://servername:3306/PLINKDB

#Derby (local)    (Experimental!):
#[PLINKDB_DERBYJDBC]
#DriverClass=org.apache.derby.jdbc.EmbeddedDriver
#URL=jdbc:derby:C:\data\derby\plinkdb

#Derby (net)   (Experimental!):
#[PLINKDB_DERBYJDBC]
#DriverClass=org.apache.derby.jdbc.ClientDriver
#URL=jdbc:derby://localhost:1527/plinkdb

#Firebird (Experimental!):
#[PLINKDB_FIREBIRDJDBC]
#DriverClass=org.firebirdsql.jdbc.FBDriver
#URL=jdbc:firebirdsql:host[/port]:/path/to/db.fdb
#example: jdbc:firebirdsql:ora10:/Dokumente und Einstellungen/Administrator/Desktop/firebird
 /data/PLINKDB.FDB#Path is relative to server without drive letter. Data has to be in the 
 same folder of the service executable.

#SQ-Lite (pldbdemo)
[PLDBDEMO_SQLITEJDBC]
#:VALS_S
#:HELP;default;IP-adress or server name, on which the database is installed
Server=localhost
#:VALS_S
#:HELP;default;The instance name of the database. Oracle: SID
ServerDB=pldbdemo
#:VALS_S
#:HELP;default;The jdbc driver class.
DriverClass=SQLite.JDBCDriver
#:VALS_S
#:HELP;default;The complete URL for the jdbc driver.
Url=jdbc:sqlite:/$CADENAS_USER/sqlite/pldbdemo.db3

For example, in the case of a PLDBDEMO installation the name PDBDEMO_SQLITEJDBC is used for database connection. This description should also be set in the PARTlinkManager under Extras --> Configure ERP environment --> tab Database.