powered by CADENAS

Manual

Manual

2.3.7.4.1. Block [AttributeMapping(is3d)]

In the block AttributMapping(is3d) you can determine whether the PARTsolutions standard attributes are to be transferred to the CAD system, and if so, in which language(s)

  • Under Attr_CopyFrom_01 set the desired language.

    • default: The attributes are exported in $CADENAS_LANGUAGE.

    • Assign language (german, english, french, etc.): The standard attributes are exported in the indicated language.

      [Note] Note

      If there is no translation for selected language of the attribute, no attribute is exported (not even from the $CADENAS_LANGUAGE language).

    • No entry: No standard attributes are transferred. (In order to explicitly export specific attributes, please see the information in the following sections.)

    Possible values for the language are:

    default,german,english,italian,french,spanish,portuguese,czech,slovak,hungarian,slovenian,dutch,danish,finnish,russian,japanese,korean,chinese,polish

    For copying attributes the parameters var_exclude and var_visbile=1can be used.

    var_visible=1 at this place tells the interface that only visible attributes have to be processed

    With „var_exclude“ you can assign certain attributes to an "Ignore" list.

    Examples:

    Attr_CopyFrom_01=default,var_exclude=A,var_visbile=1

    The variable A is explicitly set to the ignore list.

    Attr_CopyFrom_01(isCatalog(norm))=default,var_exclude=D,var_visbile=1

    Here, the expression is only applied to the standards catalog.

  • Under Attr_Prefix_01 set the desired prefix.

  • The keys Attr_Content_01 and Attr_Section_01 remain unchanged.

In Solid Edge the attributes are displayed under Part properties on the User-defined tabbed page as standard attributes.

PARTsolutions: tabbed page "AttributeMapping(3D)"

PARTsolutions: tabbed page "AttributeMapping(3D)"

Solid Edge: tabbed page "User-defined"

Solid Edge: tabbed page "User-defined"