Values
of all value range variables with names of the variables
$CHANGEABLEVALUES.
Values
of all value range variables that can be changed by user, in other
words are not locked (see common.cfg - LockDimRange=0/1)
$CHANGEABLEVALUESWITHNAME.
Changeable value range with name
$CATALOG_NAME.
Name of catalog
$CATALOG_DESC.
Visible
name of catalog (in current language)
$SHORTNB.
Short
standard description
$CADSYSTEMNAME.
Name of registered CAD system (if more than one
is registered, separate by comma)
$CALCED_ROW.
Row
number currently being calculated
$NB.
Standard name
$LINA.
BOM name
$NENN.
For DIN
912 z.B. $d.x$L. (only for standard parts, not catalogs)
$NORM_NUMBER.
Standard
number of a part
Located in the tab file; can be seen in
PARTeditor -> Identification specifications or in index
tree
$NORM_TITLE.
Standard title
of a part
Located in the
tab file; can be seen in PARTeditor -> Identification
specifications or in index tree
$MATERIAL_NAME.
Material (internal name) from material
dialog during export (see PARTdataManager -> Extras -> Settings -> Register PARTdataManager
-> Choose material on export; may be turned on/off)
(Attention:
For ERP functionality content, additional column
needed)
$MATERIAL_DESC.
Description text for material
(Attention: For ERP functionality
content, additional column needed)
$VARNAME.
Variable name
(For example,
in PARTadmin
and PARTlinkManager in the ERP settings
for the declaration of a standard name or in PARTdesigner, PARTproject in the row
description)
Syntax for
the variable description is:
$VARNAME(SRC=VARDESC).
Syntax for the value description
is:
$VARNAME(SRC=VALDESC).
Syntax for the unit is:
$VARNAME(SRC=VARUNIT).
In addition, you can state the language
optionally:
$VARNAME(SRC=VARDESC;LANGUAGE=german).
$VARDESC.
Variable
description
$VALDESC.
Variable's value description
$VARVALUE.
Variable value
$LISTOFCOLUMNS.
Display of
list with variable values of current row. The format of the
display may be influenced.
Example:
$LISTOFCOLUMNS(COLTYPE=ALL;EXCLUDE=D,L;
VALUE=$VARNAME.=$VARVALUE.)
COLTYPE
ALL All Variables
VISIBLE All visible variables
ERP All ERP variables
EXCLUDE List of variables, which shall not be displayed
INCLUDE List of variables, which shall be displayed
in addtion to the ones specified by COLTYPE
VALUE specifies how variable data
shall be displayed
The following placeholders
can be used
$VARNAME. Variable name
$VARDESC. Variable description
$VALDESC. Variable's value description
$VARVALUE. Variable value
CURRENTVARSET
Used in order
to uniquely identify a row.
The variable
CURRENTVARSET contains current values of all variables. It can be
used to transfer parameters to a website, for example.
The
variable CURRENTVARSET can be specified by different type
declarations.
Example:
$CURRENTVARSET(type=ERP_VARSET,MAXLENGTH=4000)
Possible types are:
COMPLETE
ERP_VARSET
ERP_COMPLETE
ERP_UPDATE
SHORT (compact varset, sufficient
to find a row)
XVARSET (only value ranges)
The types ERP_* and SHORT support the
"MAXLENGTH" parameter in addition.
The types
ERP_* support a parameter PINDIMVARS (value range 0/1). PINDIMVARS
controls, whether dimensioning variables shall be included in the
varset, which is not the case by default.