powered by CADENAS

Manual

Manual

4.14.3.1. Online replication

  • As soon as data are already available with the number in the LinkDB, the identification of datasets using the number is offered; this is absolutely clear.

  • In the ERP-System or the PDM-System, which takes over ERP assignments, a trigger (SAP: BAPI) takes care of the transfer of data changes into Part Solutions.

  • The trigger calls up PARTdataCenter with the dataset to be updated; PARTdataCenter adds the dataset in the LinkDB.

  • Triggers must be written especially for the existent ERP system.

The data are read in from a CSV file.

The only requirement is that the corresponding ident number is already available in the LINKDB.

Results in PARTdataManager: