powered by CADENAS

Manual

Manual

1.3.3.1.5. Check project changes in detail (after the installation)

After the installation you can check project changes in detail in the PARTdataManager under Part selection -> History -> Installed catalogs.

Here you can see which catalogs have been added and which files have been changed in compare with the previous version.

The following icons are signalizing the respective directory or project status:

Changes / New files in the directory

On directory level: All projects in this directory are unchanged.

Project level: No changes, identic project

The file has changed / Changes in the project

The file is new / New project
Project deleted

The following figure shows an example.

Open modification history via mouseover.Via configuration file the display of the history can be set on and off. See under Änderungshistorie von Installationsverlauf an-/ausschalten.

Open modification history via mouseover.[3]

As soon as you move the mouse over an icon, a tooltip with the history of changes is shown.



[3] Via configuration file the display of the history can be set on and off. See under Section 1.7.4.6.1.8, “ Key "ShowInstallHistory" - Show/hide Installation history ”.