Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
You can transfer any third party information to PARTsolutions with ERP integration (into the link database).
In the context PARTsolutions with ERP integration there are three basic requirements concerning data transfer and integration:
Cyclic data update can be
processed by the script nightupdate.vbb
. Details on this can be
found under Section 4.14.3.5, “
Configuration file nightupdate.cfg
”.
The identification of the correct dataset can happen by the material master number and the ERP_PDM_NUMBER.
Once a dataset is clearly assigned, then information from any ERP columns can be transferred into the link database.
The following figure exemplifies an update of the columns Price and Inventory.
The license "CSN2005*PSDEV*PIDENT" has to be available.
The ERP system cyclically exports changes in form of a CSV file (e.g. daily, possibly several times a day, usually by night. The CSV file only contains datasets changed during the last cycle.
Via scheduled task a job is defined (according to the export-cycle from the ERP system).
Thereby the
script nightupdate.vbb
is called
up; either with or without additional declaration of the configuration
file:
Without explicit declaration of a configuration file:
"%cadenas%\bin\x86\32\cscripthost.exe" "%cadenas_setup%\scripts\erp\nightupdate.vbb"
With additional declaration of a configuration file. This can make sense, if differently configured CSV files are used.
"%cadenas%\bin\x86\32\wscripthost.exe" "%cadenas_setup%\scripts\erp \nightupdate.vbb" "nightupdate.cfg"
The script
is stored under $CADENAS_SETUP\scripts\erp\nightupdate.vbb
.
Please also regard notes in the script file itself.
The
configuration file is stored under $CADENAS_SETUP\nightupdate.cfg
.
In the
configuration file nightupdate.cfg
specific
adjustments are performed.
The changed datasets of the third party system are written into the LinkDB according to these settings.
Note | |
---|---|
Detailed
information on the configuration file |
Note | |
---|---|
Detailed information on updating the search index can be found under Section 4.5.10, “More information” -> "Automatic index updates". An older
concept is an update via scripting. (See |