powered by CADENAS

Manual

Manual

4.17.3.1. Background information

PARTsolutions offers the opportunity to connect ERP systems via a link database. This database contains ERP data such as for example, article numbers, material, inventory, prices, etc.

This enables additional ways to represent customized business processes.

Precondition is, that the value range variables are specified by the catalog supplier according to the categories of Identification type, because only in this way an error free use of this, and the resulting NB and LINA can be secured in the ERP system. For details please see Section 9.8.11, “ Identification type ” in eCATALOGsolutions Manual.