powered by CADENAS

Manual

Manual

1.7.5.18.8.1. Key "ClassIdsSkipErp"

Always show holes (without ERP integration as well) regardless whether button "Preferred rows on/off" is activated or not.

Normally holes are not managed via ERP. Meaning that these are "red" and thus are hidden when (Vorzugsreihen an/aus) is on.

"Preferred rows on/off" in ERP toolbar

"Preferred rows on/off" in ERP toolbar

"Preferred rows on/off" button in "Default toolbar"

"Preferred rows on/off" button in "Default toolbar"

Because this behavior normally is not desired, all classes of holes are explicitly specified in the key "ClassIdsSkipErp" and thus exclude from filtering.

[Hinweis] Hinweis

The setting has to be performed in the configuration file under %cadenas_setup%/partconnection.cfg for each desired type of connection [section] always in the key ClassIdsSkipErp.

The holes are already listed per default.

[ThroughHole:ThreadNutside:CommonOuterdrive]
ClassIdsBoltside=HOLES_COMMON_THROUGHHOLE,WASHER,LOCKWASHER,BOLTS_COMMON_OUTERDRIVE
...
ClassIdsSkipErp=HOLES_COMMON_THROUGHHOLE,HOLES_COMMON_THROUGHHOLETHREAD
...
...

Result in Verschraubung dialog area:

Connection dialog: "Preferred rows on/off" OFF

Connection dialog: "Preferred rows on/off" OFF

Connection dialog: "Preferred rows on/off" ON: Holes are displayed - although "red"

Connection dialog: "Preferred rows on/off" ON: Holes are displayed - although "red"