Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.3.3. CoCreate Modeling Integration - Administration
2.3.3.4. Block
[AttributeMapping(is3d)]
|
|
---|---|
Zurück | Weiter |
PARTsolutions variables (geometric, NT, NN, LINA, etc.) and all fields in the link database (if an ERP connection exists) can be transferred to CoCreate Modelling or Creo Elements/Direct Modeling via attribute mapping.
Attribute mapping is controlled by the following blocks:
In the block [AttributeMapping(is3d)] you determine whether the PARTsolutions standard attributes (geometric, NT, NN, LINA, etc.) are to be exported to the CAD system and if so, in which language(s).
Under Attr_CopyFrom_01 set the desired language. The keys Attr_Content_01 and Attr_Section_01 remain unchanged.
default: The attributes are exported in English.
Assign language: The standard attributes are exported in the indicated language.
default,german,english,italian,french,spanish,portuguese,czech,slovak,hungarian,slovenian,dutch,danish,finnish,russian,japanese,korean,chinese,polish
Hinweis | |
---|---|
If there is no translation for the indicated language of the attribute, no attribute is exported (not even from the german language). |
No entry: No standard attributes are exported. (In order to explicitly export specific attributes, use the other sections.
Zurück | Nach oben | Weiter |
2.3.3.3.2. Key "replace_char" - Ersetzen von Zeichen | Zum Anfang | 2.3.3.4.1. Key "Attr_CopyFrom_01" |