powered by CADENAS

Manual

Manual

1.5.1. How can I select catalogs and product groups?

  1. Select desired catalog or directory.

    [Note] Note

    Specific depiction depends on portal. On the level of Home directory you can see subdirectories of the root directory.

    If only the own company catalog is available, product groups are already displayed. If several catalogs are available, then these are offered in a first step.

    When selecting the Home directory, on the left, a selection option by first letter is displayed. When clicking on a letter the respective catalog area is shown. There, select the desired catalog. The bar is hidden after a few seconds, however when starting scrolling shown again.

    Exemplary catalog selection on B2B portal

    Exemplary catalog selection on B2B portal

    Exemplarily, first directory level after selection of Ganter catalog

    Exemplarily, first directory level after selection of Ganter catalog

    [Note] Note

    When browsing through the directory levels, click on logo/icon or name.

    With Back you return to next higher level.

    With Home you will reach the uppermost level.

  2. Select product groups as long as a concrete part or assembly is specified.[1]

  3. Once selecting the part or assembly , the Table view is opened (depending on portal possibly Variable view [table view left out]).

    Product level opened

    Product level opened

[Note] Note

Component specification (characteristic) is performed in table view or variable view.

TagCloud

The TagCloud is displayed on all directory levels (depending on portal) and shows the most frequently used terms of selected product or directory. When clicking on a term, a search is directly started and the results are listed. The font size is in relation to the frequency of terms.



[1] On B2B portal, you have to be on page 3D CAD CATALOGS.