powered by CADENAS

Manual

Manual

4.5. Post-installation/update of catalogs (standard and supplier part catalogs)

[Note] Note

Make use of catalog updates. In this way best part quality is ensured.

Via PARTupdate you can be notified on updates. On this see Section 4.5.2, “ PARTupdate - Notification on available catalog updates ”.

[Note] Note

The downloading of catalogs (*.cip) is only possible for approved customers with valid maintenance.

For verification please send an e-mail to:

sekretariat@cadenas.de

Specifying:

Company, zip code, location, first and last name of the employee + e-mail address, which is used to login. As subject please enter "Verification of user data".

During the initial installation the dialog for the selection of Standard part catalogs appeared in the installation routine.

Standards selection

Standards selection

You could select from the following Standard catalogs:

  • AIA NAS: Aerospace Industries Association Standards (AIA) and National Aerospace Standards (NAS)

  • ASME: Standards of the American Society of Mechanical Engineers

  • MS Library

  • NHS

  • AS (AEROSPACE)

  • ASNA (AEROSPACE)

  • ANSI: American Standards

  • BSI: British Standards

  • CSN / STN: Czech Slovakian Standards

  • DIN-EN-ISO (linked)

  • DIN: German Standards

  • EN: European Standards

  • GB: Chinese Standards

  • GOST: Russian Standards

  • ISO: International Standards

  • IS: Indian Standards

  • JB:Chinese Standards

  • JIS: Japanese Standards

  • KS: Korean Standards

  • LN (AEROSPACE)

  • MS (AEROSPACE): Military Standards MilSpec under parent organization of ANSI

  • NAS (AEROSPACE)

  • NASM (AEROSPACE)

  • NSA (AEROSPACE)

  • NF: French Standards

  • NF-EN-ISO (linked): French-European Standards

  • NSA (AEROSPACE)

  • PN: Polish Standards

  • UNI: Italian Standards

  • UNI-EN-ISO: Italian-European Standards

  • VG (AEROSPACE)

In order to post-install missing catalogs or to update already available catalogs (Standard catalogs or Supplier catalogs) use the online installation via PARTadmin.

You can call PARTadmin -> Catalog update -> Online directly from PARTdataManager.

When clicking on the button PARTadmin opens.

Post-installation / update of catalogs

Post-installation / update of catalogs

At the desired catalogs, activate the checkbox and click on Download/install selected catalogs.

[Important] Important

It is expressly recommended, in the dialog area 3. Versions, either to choose the option Keep all or the option Number of versions >=2 (default 2).

Details on catalog updates can be found under Section 1.3.3.1, “ Catalog update Online ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.

For catalog new installations, of course you can install from DVD, too. On this see Section 3.1.2.1, “3D catalog selection: Standard and supplier part catalogs ”. Possibly the DVD catalog status is not up-to-date, so that actually the online update is the preferred option.

With existing ERP integration please regard the notes under Section 4.5.3, “Catalog update with ERP integration” in addition.

Notes on the relation between software and catalog (Lucene index) status can be found under Matrix: Software- und Lucene-Index-Version.