powered by CADENAS

Manual

Manual

2.2. System requirements

A proper operating of PARTsolutions within WINDOWS is only warranted in combination with system requirements mentioned below. An installation on other systems is possible with reservations, but will not be supported.

Which systems are possible?

  • For client operation of software (e.g. PARTdataManager) the following systems can be used:

    • Windows 7

    • Windows 8 (as of PSOL V9.08 SP0)

      [Note] Note

      On this please regard the CAD specific system requirements. Support is given, if the respective CAD interface also supports Win8.

    • Windows 10 (as of PSOL V10.00 SP2)

      [Note] Note

      On this please regard the CAD specific system requirements. Support is given, if the respective CAD interface also supports Win10.

  • For server operation of software (e.g. Server of a Client-Server Installation, PARTapplicationServer, License manager) the followings systems can be used:

    • Windows Server 2008 R2

    • Windows Server 2012

      (corresponds to Windows 8)

      [Note] Note

      On this please regard the CAD specific system requirements. Support is given, if the respective CAD interface also supports Win8.

    • Windows Server 2012 R2

      (corresponds to Windows 8.1)

      [Note] Note

      On this please regard the CAD specific system requirements. Support is given, if the respective CAD interface also supports Win8.1.