powered by CADENAS

Manual

Manual

3.2. Client-Server Installation

The installation routine will guide you carefully through the installation process.

However, we request you to regard the following information.

A Client/Server-Installation installs the entire PARTsolutions Software and the corresponding Catalogs onto a server computer in the network (file server). The Client workstations are then only available in the respective relevant PARTsolutions program parts.

The installation takes place in two steps:

  1. Server installation

    Catalog installation and installation of PARTsolutions packages.

  2. Client installation

    Individual selection of client-sided required PARTsolutions packages.

    (The catalog display can be individually suppressed later via PARTadmin -> Index administration if needed. See Section 1.1.3.4.5, “ Context menus” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual)