powered by CADENAS

Manual

Manual

3.1.1.20. Online registration and Licensing

At this point you have the opportunity to order the required licenses online as well as register. Needed are: Internet browser and access.

  1. When you want to order licenses online, then please confirm with Yes.

    -> The online connection is set up and the respective form appears.

  2. For "No" skip the following information.

[Note] Note
  • Preferably use the form at this place for ordering a single workstation license, when you sit in front of the respective computer. In this case the host ID is automatically detected and inserted in the form.

  • If you need several single workstation licenses for different computers, then you should already have detected the MAC addresses of these computers before, because you have to manually insert them in the form.

    Of course you can also carry out the registration or Licensing later. Then call up the online form under $CADENAS/log.

  • In order to order a single workstation license, you can call up the form via PARTadmin -> category License administration -> subitem Clients -> index page Request licenses online. Also in this case the host ID is already automatically inserted in the form for the respective computer. See also Section 5.4, “ Licensing”.

  • In order to order FLM licenses, call up the form from PARTadmin -> category License administration -> subitem FLM server -> index page Request licenses online. See also under Section 3.4.6, “Request/Import FLM licenses ”.

  1. Fill out the marked fields (red asterisk).

  2. Enter the registration card number [3]

  3. Set the license type [4]

--> The network card number is automatically determined and entered.

  1. In case you want to set up the same program configuration on other computers, click on Add Computer.

  2. Send data to CADENAS.

Licensing form - section 1

Licensing form - section 1

Licensing form - section 2

Licensing form - section 2

Licensing form - section 3

Licensing form - section 3

[Note] Note

Please regard the licensing information in the FAQ section under Section 5.4, “ Licensing”.



[3] The registration card number (14-digit registry number) can be taken from the installation documents, which you received along with the DVDs.

[4] In case you installed dongle drivers you must enter the dongle ID in the section for the network card. For this the dongle must be inserted in the respective port.