Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
4.7. Catalog
(standard and supplier parts catalog) post-installation / update
4.7.3. Catalog -
Update
|
|
---|---|
Prev | Next |
During a catalog update old and new versions are compared. This process follows the scheme below:
Points 1 and 2 are always carried out, even if no ERP integration exists.
The following point is only of importance if an ERP integration exists. See Workflow - Katalogupdate.
Compare the project rows with changes in the columns "ACTIVE_STATE" and "REQUESTED_STATE"
When checking the project rows, the following may occur:
Rows without connection to the LinkDB
Additional project rows may not have a connection to the LinkDB. Another check takes place.
Rows with connection to the LinkDB
For all project rows which have a connection in the LinkDB an exact check of the changes (Project, table, geometry) May take place.
In addition, before the update, it is determined which of the columns "ACTIVE_STATE" and "REQUESTED_STATE" are to be kept in the LinkDB.
The following flow chart displays the steps in a catalog update: