powered by CADENAS

Manual

Manual

2.3. Hardware requirements

GROUP

Hardware requirements

CPU

Usual standard, multicore processor

The more users accessing at the same time the more cores (<25 = 8 cores, otherwise 16)

RAM

PARTsolutions: Recommendation min. 4GB

Disk space

5 GB HDD (per installed system)

Software Integration

0,1 GB HDD

Data standards & catalogs (including index)

The index takes approximately 1/5th of the space. The proportion varies greatly because the index size depends on several factors such as part type or number of translation languages.

The storage space depends on the individual requirements. The following specifications should simplify an estimation.

  • Currently available catalogs: About 880[a]

  • Annual growth of catalogs: ca. 40

  • If you plan on installing all catalogs, you need 40 GB storage space for the index and 200 GB for the catalogs.

  • If catalogs are on a network drive, the index should be cached locally, meaning additional storage space is required, which is according to the index size.

FLM server

0,1 GB HDD

Graphics card

Minimum 64 MB; OpenGL-capable; Hardware 3D assistance recommended

[Note] Note

As resolution 1280x1024 is required as a minimum.

Connectivity WIN - UNIX NFS or Samba

[a] State 10/2020