powered by CADENAS

Manual

Manual

3.1.2. Installation of catalog and pool data DVDs

[Note] Note

Due to amount of data, the catalog files are divided among several DVDs.

Please insert the first PARTsolutions- Catalog and Pool Data DVD into the respective CD-ROM drive. Should the installation routine not start automatically, double-click on the file CDROM:\Setup.exe in the Windows Explorer.

--> Now you will be guided through the installation process

[Note] Note

Follow the instructions of the installation program. Defaults and specific paths may vary slightly from the printed text.

[Note] Note

Concerning Uninstall catalog or Cleanup versions see also Section 1.3.4, “ Index administration ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.