Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Columns can be provided with the feature to start a program or to open a document when clicking into the column. Define the respective column under PARTproject -> General1 -> Variables -> Variables containing external references. After this it is highlighted in green.
Define the document which shall be opened when clicking on the defined column.
The document (also several for different languages) has to be stored in the project directory.
If documents are available in several languages attach a language ID to the file name separated by an underscore. In the example below "_english" and "_german".
In PARTproject -> General1 -> Variables -> Variables containing external references -> Document to open set the following entry:
info_$CADENAS_LANGUAGE..txt[25]
Define the program (*.exe) to be opened when clicking on the defined column (WIN)
Program to be carried out (UNIX):
Define the program (*.exe) to be opened when clicking on the defined column (UNIX).
[25] The two points one after another are correct: The first point belongs to the variable declaration.