powered by CADENAS

Manual

Manual

6.3.4.1.2. Dimensioning *.3db Object

  1. You can dimension the *.3db object using the buttons in the bottom toolbar of the new 2-D drawing window.

  1. Move the mouse pointer to the Vertical dimensioning at 2 points until the snap appears and click to set.

  1. Move the mouse pointer to the first line until the snap appears and click to set.

  2. Repeat this step to create the second line.

    --> The dimension lines become visible at the mouse pointer.

  1. Draw the dimensioning line at the desired position und fix it by mouse click.

    --> All dimensioning elements and the menu window Change parameter become visible.

  2. Define the Offset value (dimension to reference axis) and the Height (Type size) of dimension (see fig.).

  3. Dimensioning text:

    Default is "{AUTOMATIC%0}" with curly braces. (In the above example "%0", so that "8" without decimal places is displayed as dimensioning number.

    "AUTOMATIC" takes the current value from the geometry. (Not recommended).

    Define a static, dynamic or mixed static-dynamic Measure text.

    Using %"number" you can define Decimal digits. (For example: A={A%2})

    Dimensioning text: static

    Dimensioning text: static

    Add any static text.

    dimensioning text: static - dynamic

    dimensioning text: static - dynamic

    Connect the two options.

    Dimensioning text: dynamic

    Dimensioning text: dynamic

    Now enter the desired variables. The desired value is dynamically generated.

    Dimensioning text - 3 possibilities

    Dimensioning text - 3 possibilities

    [Note] Note

    To satisfy high design demands, you can create external preview pictures and provide it as *.pra file for example. On this see Section 5.5.2, “Import DWG/DXF files and convert them into .pra format”.

    Dynamic generation of the variables content in the measure text is only possible like described above!

  4. Click on the Accept changes button.

  5. Close the 2-view.

    The new created view will be displayed in the "History" menu.

    -> The dimensioning image is now available as 2-D view in PARTdataManager.

    PARTdataManager- Dimensioning views

    PARTdataManager- Dimensioning views

Delete...

The "Delete" command is found in the context menu of the respective "History" item.