powered by CADENAS

Manual

Manual

13.9.4. Rule – pipe clip

  1. Dialog area Configurator: Open the context menu of the connection point "pipe clip" (right-click).

  2. Select New rule….

  1. Define a name and a rule between pipe clip and pipe center.

  2. Dialog area Assembly: Open the context menu of "pipe clip" (right-click).

  3. Select Insert pipe clip (ex.) and the first characteristic from the table.

    --> In the Configurator dialog area, the rule for the connection point "pipe clip" has been inserted.

    --> In the Assembly dialog area, a characteristic of the pipe clip start element is already located.

    --> The 3D preview of the pipe clip start element shows up.

  1. Dialog area Configurator: Open the context menu of the "pipe clip (R)" by right-clicking.

  2. Select Variable shares... .

  1. First click on the button Commit.

  2. Then double-click the button next to Share name .

    --> The input fields are active.

  1. Share nameAssign H1 for the first .

  2. Click on the Browser-Button.

  1. --> The Variable browser is opened.

    Allocate "KP1" and "H1" to each other.

  1. Apply (as described above) another row. Call this "s2" and make the following allocation:

    "AP" --> "S2"

    --> Finally these two rows must be entered.