Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Under
$CADENAS_SETUP/layouts/2dderivation
set up your own dw file (or copy an existing one and modify
it).
Under "name", assign a unique name.
[Template] name=drawing_3_views_eu_test1 unitbase=mm [Description] default=Test 1 german=Test 1 [ELEMENT_grid1] type=grid padding_x=10 padding_y=10 padding_unit=percent columns=2 rows=2 order=none,top,front,left
Select a part and in the toolbar click on the 2D derivation button.
Note | |
---|---|
Concept for use of frames and different paper formats: Via [ELEMENT_frame] in the template file *.dw a default frame can be defined. If views for different paper formats are to be created, a separate configuration file is defined for each format via [Formats]. The configuration file in turn references to a specific dxf file (paper format) under [ELEMENT_frame]. |