powered by CADENAS

Manual

Manual

13.7.2.4.3. Define second condition

A second Condition should make sure that the Length of the butterfly screw is oriented to the Thickness of the plate. The screw may never be shorter than the plate height of + 4mm.

In menu Condition properties the expression PL@H+4<=FS@L has to be stated.

For exact steps, see Section 13.7.2.4.2, “Defining first condition ”.

--> Dialog area Configurator: The second condition (if) Length shows up. --> In the 3D preview only combinations will now be displayed at which the screw length tops the plate height by at least 4mm.

Considering the Table you can see the effect [58] of the second condition.

If you select a plate with the height of 6 mm,...

...only butterfly screws with at least 10 mm length are available.



[58] You have to select the appropriate assembly element.