Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The "Template" element contains basic information and is mandatory.
It contains the following attributes:
Name is the unique identifier for this sketch view. In other words, there may not exist another one by the same name.
Indicates the basic unit in which the sketch view is defined.
hide (if not available, set the attribute by yourself)
With "hide=1" you can prevent the display of template under PARTdataManager -> 2D derivation -> Combination views.
[Template] name=drawing_3_views_eu unitbas hide=0/1
You can also use cuts in 2D views.
Therefor specify sectional plane, cut direction (1/-1) and optionally offset in the block Template.
[Template] cutPlaneType=YZ cutPlaneDirection=1 cutPlaneDistance=0.0
Under "order", enter the desired views to be displayed:
[ELEMENT_grid1]
type=grid
padding_x=10
padding_y=10
padding_unit=percent
columns=2
rows=1
order=back,left