Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Create a new sketch to create the inner thread.
Note | |
---|---|
Not until a Rotation axis has been defined, are the Cylindrical thread by length and Conical thread by lengths buttons defined! |
Click on the respective sketch elements and areas and follow the notes in the footer:
The Change parameter window opens. Insert 'T-X' for the Thread length and 'X' for the Run out length. |
|
Select Cut -> Rotate... in the context menu of sketch 3 and confirm with OK in the Rotational solid window.
--> In the 3D view menu area the finished cap nut is displayed.
Insert the Filenames and/or the storage location and save the file. --> The Part information menu[6]will open.
If needed, change the available entries and confirm with OK. --> Thus the cup nut geometry is finished.
Note | |
---|---|
In order to show the Geometryin the Preview, first you have to click another feature in the Project selection menu, and then again the cap_nut.3db-file . |
Note | |
---|---|
Further information on the creation of an outer thread with different variants of thread pitch is found under Section 7.5.4.3.11, “ Threads ” . |