Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The CADENAS classification (Classification (CNS)) is used for the following:
Placement information, published elements and attributes
Assigning of elements happens in the PARTdesigner.
Detailed information on this is found under Section 5.9, “ Published elements ”.
Transfer physical properties (especially Volume, Mass, Density, Material)
For the assignment of physical properties, object attributes and geometrical attributes proceed as follows:
Under Classification (CNS), click on the search button .
Under Attributes (CNS) click on the search button .
-> The dialog box Class variables opens.
All attributes are listed here.
Placement attributes have the identifier CNS_CP_PLACE_PA in the column "Class".
Object attributes have the identifier CNSERPBASE.
Physical attributes have the identifier CNSPHYPROP.
In the column Variable, you can assign variables, in the column Value, fixed values.
When exporting to the CAD system all classification attributes are transferred. In the PS3 file you can find these in the section "CLASSIFICATIONINFO".
Information on how the physical attributes are analyzed, you can find in the PARTsolutions User manual in the respective CAD specific section under "Physical properties from PARTsolutions".
It would be an alternative concept using Standard variables directly in the table instead of using Class variables. Compare Section 11.5.2.2.4.1, “ Standard variables ”.