Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The "Grid" element is declared as "ELEMENT_" followed by a unique identification for that element.
[ELEMENT_grid1]
The following attributes are available:
Defines the space between the individual derivations in the y plane (see red marking in above image)
Defines the space between the individual derivations in the x plane (see red marking in above image)
Defines the unit in which the space is given. Currently only possible in PERCENT (based on box width).
If a parent is assigned, the grid aligns its breadth/height according to its parent. Without parent element, the grid takes up the entire space.
The following parent elements are possible:
box (see Section 8.4.4.5, “[ELEMENT_box] as wildcard element ”)
Constructs a wildcard element.
The value is for example parent = box1, if the [ELEMENTE_grid1] in the [ELEMENT_box1] is to be embedded. See example 2 below.
frame (see Section 8.4.4.9, “[ELEMENT_frame] Combine more elements in frame ”)
If no box is being used as parent, the entire available space is used. The size of the grid CANNOT be changed in Edit mode. |
If a box is being used (see Section 8.4.4.5, “[ELEMENT_box] as wildcard element ”), it can be selected in Edit mode and the size maybe changed. |
[Template] name=grid_ohne_box unitbase=mm [Description] default=Grid without box german=Grid ohne Box english=Grid without box [ELEMENT_grid1] type=grid padding_x=10 padding_y=10 padding_unit=percent columns=2 rows=2 order=top,none,front,left
|
[Template] name=grid_mit_box unitbase=mm [Description] default=Grid with box german=Grid mit Box english=Grid with box [ELEMENT_box1] type=box align=center position_x=20 position_y=20 position_w=230 position_h=245 [ELEMENT_grid1] type=grid parent=box1 padding_x=10 padding_y=10 padding_unit=percent columns=2 rows=2 order=top,none,front,left
|