powered by CADENAS

Manual

Manual

7.8.18.1. Media Variables for tooltip information on PARTcommunity

In this section you can find a description on how to create Media Variables used in PARTcommunity for the display of tooltip information.

When clicking on the info icon, a tooltip with additional information is opened.

When clicking on the info icon, a tooltip with additional information is opened.

Naming of Media Variables has to be according to the following schema:

The Media Variable allocated to the table variable has the same name + "_HELP"

Tablevariable_HELP

Example:

If you want to create a HELP variable related to a table variable BNEB then the name of the Media Variable has to be BNEB_HELP.

The exact procedure is described in the following: